IMXRT1176 100MSPS Parallel ADC question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1176 100MSPS Parallel ADC question

Jump to solution
1,952 Views
VinGanZ
Contributor III

Hello

I am trying to interface a 16 bit 100MSPS parallel ADC with the Flexio port of imxrt1176. Is this feasible?

kind regards

Vinod Ganesh

0 Kudos
Reply
1 Solution
1,931 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
The FlexIO clock frequency of i.MX RT can up to 120 MHz.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,943 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is this feasible?
-- In my opinion, it's feasible.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,941 Views
VinGanZ
Contributor III

Thank you for the information. Could you also confirm that the maximum flexio clock which is 120MHZ as per reference manual is also the maximum parallel port speed possible?

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

0 Kudos
Reply
1,932 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
The FlexIO clock frequency of i.MX RT can up to 120 MHz.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply