Debug issue in IMXRT1170 EVK kit and USB1(SDP) as UART USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug issue in IMXRT1170 EVK kit and USB1(SDP) as UART USB

ソリューションへジャンプ
798件の閲覧回数
Naveed
Contributor II

Hi,

1. We are using MCUXpresso IDE for bringing up of IMXRT1170 EVK kit and facing debugging issue as attached. Please find the attached image.

2. We are using MCUBootutility tool to load binary file to flash into the IMXRT1170 EVK board and able to load using USB HID but not with USB UART , for our application we required USB UART  how to configure for accessing USB1(SDP) as UART console( presently we can use J20 as USB HID ). We referred  this link https://developer.embeddedartists.com/docs-mcu/howto/nxp-mcu-ota/#sbl

Thanks in advance.

Naveed_0-1664273542761.png

Naveed_1-1664273616908.png

 

 

0 件の賞賛
1 解決策
749件の閲覧回数
jay_heng
NXP Employee
NXP Employee

J20 is I.MXRT USB OTG1 port, it is not UART console port mentioned in the post.

The UART console is from On board DAP-Link debugger Port J11, it contains USB to UART function.

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
775件の閲覧回数
jay_heng
NXP Employee
NXP Employee

What do you mean about USB UART? You want to load binary via UART?

0 件の賞賛
767件の閲覧回数
Naveed
Contributor II

Naveed_0-1664282236318.png

https://developer.embeddedartists.com/docs-mcu/howto/nxp-mcu-ota/

Yes, we referred the above instruction to flash the sfw092.bin into the IMXRT1170 EVK Flex SPI NOR flash as attached from MCU Boot Utility tool and also shared the link and followed all the steps, but PC is not able to detect the UART port which is connected to J20 interface so unable to get the output in the console.

Will you let us know where we have missed anything in the configuration, that will be helpful.

Thanks in advance.

 

0 件の賞賛
750件の閲覧回数
jay_heng
NXP Employee
NXP Employee

J20 is I.MXRT USB OTG1 port, it is not UART console port mentioned in the post.

The UART console is from On board DAP-Link debugger Port J11, it contains USB to UART function.

0 件の賞賛