Could I use DCD to initialize HyperRAM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could I use DCD to initialize HyperRAM?

775 Views
BlackTurbo
Contributor III

Hi, I'm using RT1062 for a GUI application, the hardware design is NAND+HyperRAM. Right now I'm using a second bootloader to initialize HyperRAM and DCD to initialize the NAND flash, could I use DCD for both the HyperRAM and NAND initizlization?

0 Kudos
Reply
1 Reply

764 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Could I use DCD for both the HyperRAM and NAND initialization?
-- No, I'm afraid not.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply