Can't access SD card with imxrt1064 using emFile system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't access SD card with imxrt1064 using emFile system

439 Views
Dhara
Contributor I

Hello,

I am trying to read and write .txt file and .jpg file, which is present in SD card, mounted on imxrt1064 EVK board. In MCUxpresso I am using inbuilt code with emFile System. according to emFile user manual porting all dependencies and all parameters done, but it not able to do FS_Fread() or FS_read().

If any idea about how to access SD card in imxrt1064 from mcuxpresso using emFile system then please share and give any suggestions related to this.

Labels (1)
0 Kudos
1 Reply

423 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Dhara,

There is not an example for emFile on the SDK. There are, however, some SD card FatFS examples. I mention it in case it may help.

My apologies for the inconvenience.

Regards,
Gustavo

0 Kudos