CSI Unused Data Input Pull-Down

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CSI Unused Data Input Pull-Down

ソリューションへジャンプ
704件の閲覧回数
jaredm
Contributor III

We are developing hardware using the RT1052 and 12-bit CMOS sensor. The RT1052 uses the CSI in 16-bit Bayer mode, the 12-bit sensor is connected to data[11:0], and data[15:12] are unused. When receiving pixel data, we would like data[15:12] to be 0's (to avoid an additional software masking step.) We have two options:

1. Connect BGA pads for data[15:12] to GND.

2. Leave BGA pads for data[15:12] NC, and enable the internal pull-down.

Option 2 is preferred, but it is unclear whether it will work.

On the RT1052 device, does the peripheral logic override the I/O pad options? Or can the I/O pad options be configured independently from the peripheral logic? For instances, can registers IOMUXC_SW_PAD_CTL_PAD_GPIO_AD_B1_04:07 be configured to enable pull-downs, even when the signals are used as peripheral function CSI data[15:12]?

Thanks in advance.

 

0 件の賞賛
1 解決策
690件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jaredm,

You may setup the pin pad regardless of the peripheral function as to enable the internal pull-downs.

These internal pull-down resistors would allow for low input read on the floating pins in some scenarios, but since these internal pull downs are weak, the input value may be affected by noise, so it’s not recommended for critical signals. I would recommend tying to ground as to make sure that you won’t have unwanted values on your application under any operating conditions.

I hope that this information helps!

Regards,
Gustavo

元の投稿で解決策を見る

0 件の賞賛
1 返信
691件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jaredm,

You may setup the pin pad regardless of the peripheral function as to enable the internal pull-downs.

These internal pull-down resistors would allow for low input read on the floating pins in some scenarios, but since these internal pull downs are weak, the input value may be affected by noise, so it’s not recommended for critical signals. I would recommend tying to ground as to make sure that you won’t have unwanted values on your application under any operating conditions.

I hope that this information helps!

Regards,
Gustavo

0 件の賞賛