Brownout detection on i.MXRT1064 microcontroller using MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Brownout detection on i.MXRT1064 microcontroller using MCUXpresso IDE

Jump to solution
160 Views
wavhal_m
Contributor II

Hello,

I'm using following code for brownout detection. I included fsl_pmu.h and fsl_pmu.c in the code. However, I observed that IRQ is not getting served. Kindly suggest the corrections in the code.

void Brownout_Init(void){
//Enable 1.1V brownout circuitry in the LDO
PMU_1P1EnableBrownout(PMU, TRUE);
 
//Set LDO output voltage to 1.1V
PMU_1P1SetRegulatorOutputVoltage(PMU, 0x10);
 
//Set LDO brownout offset voltage to 0.175V
PMU_1P1SetBrownoutOffsetVoltage(PMU, 0x7);
 
//Enable LDO output
PMU_1P1EnableOutput(PMU, TRUE);
 
//Enable 2.5V brownout circuitry in the LDO
PMU_2P5nableBrownout(PMU, TRUE);
 
//Set LDO output voltage to 2.5V
PMU_2P5SetRegulatorOutputVoltage(PMU, 0x10);
 
//Set LDO brownout offset voltage to 0.175V
PMU_2P5SetBrownoutOffsetVoltage(PMU, 0x7);
 
//Enable LDO output
PMU_2P5EnableOutput(PMU, TRUE);
 
NVIC_EnableIRQ(PMU_EVENT_IRQn);
}
 
void ANATOP_EVENT0_IRQHandler(void)
{
  const uint32_t status = PMU_GetStatusFlags(PMU);
 // uint16_t result = 0;
 
  if (status & kPMU_1P1BrownoutOnOutput)
  {
    // result = kPMU_1P1BrownoutOnOutput;
  }
 
  if (status & kPMU_2P5BrownoutOnOutput)
  {
    // result = kPMU_2P5BrownoutOnOutput;
  }
}
 
I'm having one more doubt, in the User Manual it is said that -
The following bitfields are not applicable on this device, and
those corresponding bits are Reserved:
• in PMU_REG_COREn register:
• RAMP_RATE
• REG2_TARG
• REG1_TARG
• REG0_TARG
• in PMU_MISC1n register: IRQ_DIG_BO.
• in PMU_MISC2n register:
• REG2_STEP_TIME
• REG1_STEP_TIME
• REG0_STEP_TIME
• REG2_OK
• REG2_ENABLE_BO
• REG1_ENABLE_BO
 
I found similar bitfields are also available in the register - CCM_ANALOG_MISC2n and this register is shared with PMU. So may I use CCM_ANALOG_MISC2n, instead of using PMU_MISC2n register? And its support is available in fsl_pmu.c?
0 Kudos
1 Solution
119 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Please refer to this post to turn on the brownout detector: Solved: Re: How to enable brownout detection - NXP Community

These fields do not apply to the device even when accessing through CCM registers since they share space.
Please refer to the driver, it uses different registers to enable and set the BO.

Best regards,
Omar

View solution in original post

1 Reply
120 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Please refer to this post to turn on the brownout detector: Solved: Re: How to enable brownout detection - NXP Community

These fields do not apply to the device even when accessing through CCM registers since they share space.
Please refer to the driver, it uses different registers to enable and set the BO.

Best regards,
Omar