Are you guys supporting imX RT1170 MCU yet?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are you guys supporting imX RT1170 MCU yet?

2,112 Views
fmabrouk
Contributor III

Are you guys supporting imX RT1170 MCU yet?

0 Kudos
13 Replies

2,102 Views
Masmiseim
Senior Contributor I

IAR seems to have 1070 support (1170 also)

/update

After you have fixed the typo (1070 to 1170).

What kind of support do you need?

Datasheet and Reference manual is released. The SDK should follow soon. The device is also supported by different compilers

0 Kudos

2,088 Views
mjbcswitzerland
Specialist V

It is possible that IAR has advanced information about a future product but nothing comes up with a search for an i.MX RT 1070, neither on the NXP site nor on search machines.

If it is the pipe-line I expect it is an i.MX RT 1170 without the Cortex-M4. Or an i.MX RT 1060 with dual-1G Ethernet.

Regards

Mark

 

2,083 Views
Masmiseim
Senior Contributor I

Hey mark,

 

for sure they have, what me surprises is, that they publishing this internals bevor NXP does.

The i.MX RT 1170 without the Cortex-M4 is called iMXRT1172 and iMXRT1171. Check table 1 in the Datasheet which was publicly released last month.

If you check the 1070 headerfile which comes with IAR it does not look like Gigabit Ethernet is supported.

regards

0 Kudos

2,108 Views
mjbcswitzerland
Specialist V

Hi

Do you mean 1170?

https://www.utasker.com/iMX/RT1170.html

Regards

Mark

 

0 Kudos

2,095 Views
fmabrouk
Contributor III

Thank you Mark! We have been in touch in the past while I was using your Modbus Library. Glad to know that you are supporting imX RT1170.

Cheers,

Farid

0 Kudos

2,080 Views
fmabrouk
Contributor III

I need some documentation/demo code for bootloader and doing an OTA firmware update for this new ImX RT MCU.

0 Kudos

2,018 Views
Masmiseim
Senior Contributor I

Hey fmabrouk,

You could start the development with the 1060 and port it to the 1170 when you receive it. As long as you don’t like to use one of the new peripherals (Gigabit Ethernet?) in your bootloader it should be very straight forward.

We started our application also with the 1060 and switched to the 1170 after receiving it.

 

Regards

1,996 Views
fmabrouk
Contributor III

Could you please advise about where I can find the bootloader for RT1060.

Thanks!

0 Kudos

1,990 Views
Masmiseim
Senior Contributor I

Mark gave you some links to utasker. As an alternative you could take a look at the bootloader from the SDK.

You can download the SDK for the 1060 (and the 1170 after it is released) from https://mcuxpresso.nxp.com

Don’t forget to add at least MCU Boot to the SDK Package, or take just the complete package. After extracting it, check the folder: boards\evkmimxrt1060\bootloader_examples

2,047 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Fmabrouk,

Technical documentation and the MCUXpresso SDK for the i.MXRT1170 will be available as soon as this family is launched, which should happen soon. You can contact your NXP Distributor for more details.

My apologies for the inconvenience!

Regards,
Gustavo

0 Kudos

2,044 Views
fmabrouk
Contributor III

how soon is that launch going to happen?

0 Kudos

2,042 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Fmabrouk,

There is not a public date that I can share on the public forums but your NXP Distributor will be able to provide more information.

Regards,
Gustavo

0 Kudos

2,074 Views
mjbcswitzerland
Specialist V

Hi Farid

Do you already have this part (or its EVK?)

I have a complete turn-key secure boot loader / OTA concept for the i.MX RT 10XX parts (including Modbus loading): https://www.utasker.com/iMX/developers.html (list of documents and video below too)


but I haven't ported it to the i.MX RT 1170 yet - mainly because I don't actually receive the HW until the 8th February 2021. Only limited customers and partners actually have the HW (the have had then for about 11 months or so).

Regards

Mark

 

 

- Boot loader concept including XiP on-the-fly decryption, clone protection or AES256 protected RAM execution.
-- Boot Loader concept flow chart: https://www.utasker.com/docs/iMX/Loader.pdf and usage reference https://www.utasker.com/docs/iMX/uTaskerLoader_TestDrive.pdf
-- Serial Loader features: https://www.utasker.com/docs/uTasker/uTaskerSerialLoader.pdf
-- Building the loader with MCUXpresso: https://www.utasker.com/docs/iMX/MCUXpresso.pdf (and video guide https://youtu.be/p_eUGo6GypY ) - the guide document explains how to use with any application (eg. SDK) and to enabling its operation with On-The-Fly decryption in 5 minutes
-- Building the loader with IAR: https://www.utasker.com/docs/iMX/IAR.pdf (and video guide https://youtu.be/XPCwVndP99s )
-- Building the loader with VisualStudio and GCC: https://www.utasker.com/docs/iMX/GCC.pdf (and video guide https://youtu.be/0UzLLSXABK8 )
Video Guide to encrypting NXP SDK examples to run from XiP memory using on-the-fly decryption and uploading with the µTasker loader: https://www.youtube.com/watch?v=5iT7KP691ls&list=PLWKlVb_MqDQEOCnsNOJO8gd3jDCwiyKKe&index=10
Video Guide to encrypting NXP SDK examples to run at optimal speed in internal RAM and uploading with the µTasker loader:
https://www.youtube.com/watch?v=fnfLQ-nbscI&list=PLWKlVb_MqDQEOCnsNOJO8gd3jDCwiyKKe&index=11
Video Guide for Embedded Artist OEM Module for i.MX RT 1062 showing precise secured application operation analysis: https://youtu.be/o7hQbOqhJoc