An equivalent circuit of GPIO_EMC about RT1021

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

An equivalent circuit of GPIO_EMC about RT1021

跳至解决方案
419 次查看
Edgard
Contributor III

Dear an Engineer in NXP,

I would like to know the equivalent circuit of GPIO_EMC pin.
Because I want to check the input mechanism.

Recently, GPIO_EMC_41 was broken, I think the electrical over stress (EOS) occurred to the pin.
I will put the 100 ohm resister close to pin in order to protect the pin from EOS.

But I wonder if the value of resister is large or not...

Thanks in advance.

Kindest Regards 
Edgard



标签 (1)
0 项奖励
1 解答
327 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Edgard,

Application Note AN5078 describes everything relating the pins on our MCUs. With respect to ESD and EMC protection, please look into AN10853.

BR,
Edwin.

在原帖中查看解决方案

0 项奖励
2 回复数
314 次查看
Edgard
Contributor III

Hi @EdwinHz 

thanks, I checked the App.Note you mentioned.

Kindest Regards
 Edgard

0 项奖励
328 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Edgard,

Application Note AN5078 describes everything relating the pins on our MCUs. With respect to ESD and EMC protection, please look into AN10853.

BR,
Edwin.

0 项奖励