Access SDRAM and SRAM in the same application on i.MX RT1024

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Access SDRAM and SRAM in the same application on i.MX RT1024

574件の閲覧回数
danielc
Contributor II

Hello Sir,

In i.MX RT 1024 reference manual Chapter 24, it describes that SEMC can support multiple external memories in the same application.We have one customer wants to implement the SDRAM and SRAM (peripheral used as SRAM interface)functions in their application.  Is there any hardware/software design guide can provided to this demand?

Regards,

Daniel

 

0 件の賞賛
2 返答(返信)

534件の閲覧回数
danielc
Contributor II

Hi Fangfang,

 

Customer wants to implement SDRAM and SRAM functions in the same application on RT1020 EVK first.

Do you have any design suggestion for customer? Thanks.

 

Regards,

Daniel

0 件の賞賛

559件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Yes, rt1024 support the application. But there is no the reference design for it.

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛