Hello Sir,
In i.MX RT 1024 reference manual Chapter 24, it describes that SEMC can support multiple external memories in the same application.We have one customer wants to implement the SDRAM and SRAM (peripheral used as SRAM interface)functions in their application. Is there any hardware/software design guide can provided to this demand?
Regards,
Daniel
Hi Fangfang,
Customer wants to implement SDRAM and SRAM functions in the same application on RT1020 EVK first.
Do you have any design suggestion for customer? Thanks.
Regards,
Daniel
Hello,
Yes, rt1024 support the application. But there is no the reference design for it.
Hope it help you. Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------