ADC ETC Issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC ETC Issues

Jump to solution
894 Views
rnicolls
Contributor III

Hi,

I'm working with the ADC_ETC module on the IMXRT1176 and using the SDK eaimxrt1176_sdk_2_11_1_2022-05-16 and have run into a couple of issues I need clarified.

1 ) I enable the DONE0 interrupt for Trig 0. I noticed, when I placed a breakpoint in the ISR, that sometimes the DONE0 flag for Trig 0 is set but sometimes it is not. I make sure to clear the flag when exiting the ISR but it seems to re-enter almost immediately. I'm toggling a GPIO and noticed that the GPIO is never set slow. Or it's at least set low for a very small amount of time. 

Trig 0 is triggered by the PIT at a rate of 1kHz. If I toggle the GPIO only when the flag is active, then I can see the GPIO toggling at 1kHz as expected.

2 ) I wanted to route the output of the PIT to Trig 0 and Trig 4 but noticed that there is no output signal for Trig 4. There is only ADC_ETC0_COCO0, ADC_ETC0_COCO1, ADC_ETC0_COCO2, ADC_ETC0_COCO3, ADC_ETC0_COCO, ADC_ETC1_COCO0, ADC_ETC1_COCO1, ADC_ETC1_COCO2, ADC_ETC1_COCO03.

Does this mean that Trig 4 through 7 for ADC 2 cannot be triggered independently? In order to trigger Trig 4 I had to synchronize it with Trig 1, but there maybe applications where it's desirable to assign priority between these two. It's also inferred in the Reference Manual that I should be able to trigger 4 through 7 independently. 

3) There's one small issue with the SDK: Members ADCHCRegisterSelect and ADCChannelSelect of adc_etc_trigger_chain_config_t are not correctly named. The former selects the LPADC HW trigger, the latter selects the associated LPADC command. The comments for these are not correct either. 

Thank you

 

 

 

0 Kudos
1 Solution
797 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @rnicolls ,

ADC_ETC0_TRIG0 ... ADC_ETC1_TRIG3 corresponding to trg0 ... trg7, see the figure "ADC_ETC block diagram" in the ADC_ETC chapter.

jingpan_0-1677382059514.png

 

Regards,

Jing

View solution in original post

0 Kudos
5 Replies
837 Views
mark_callaghan
Contributor III

I've been using the RT1062 ADC_ETC, and I expect the signal naming might be similar. The XBAR signal name for the ADC_ETC COCO associated with TRIG4 is ADC_ETC1_COCO0. 

0 Kudos
836 Views
rnicolls
Contributor III

Thank you for the reply. I thought as much but didn't get any conversions back from Trig 4 when I used ADC_ETC1_COCO0. I think there must be some other issue with how I've set it up.

0 Kudos
869 Views
mitterha
Senior Contributor I

Hi,

1) Did you place the define SDK_ISR_EXIT_BARRIER at the end of the ISR? ARM errata 838869 could be your issue or another DONE0 interrupt is enabled in the ADC-ETC chain config and you are not clearing it (or your other settings are incorrect see 2)?

2) Are you sure you want to connect the PIT -Trigger signal to the ADC-ETC Conversion Complete signals? Does not sound correct for me. Maybe your are looking for the XBAR output signals like ADC_ETC_TRIG00 to ADC_ETC_TRIG13  (which are the ADC-ETC triggers 0 to 7)?

 

3) sorry don't know your used IMXRT part. Maybe it is different for it but for the 1020 and 1050 series the second one selects the adc channel that should be converted and the first one selects the HC-register to use so the comment would be correct in this case.

 

Kind regards,

Steve

0 Kudos
853 Views
rnicolls
Contributor III

Thank you for the reply. 

It seems that ARM errata 838869 is the cause of the issue I'm seeing. 

Sorry if it was unclear, but I am using the XBAR output signals to trigger the conversion. I just can't find the one's associated with triggers 4 to 7. I tried using ADC_ETC1_TRIG0 but that doesn't seem to trigger the conversion. 

0 Kudos
798 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @rnicolls ,

ADC_ETC0_TRIG0 ... ADC_ETC1_TRIG3 corresponding to trg0 ... trg7, see the figure "ADC_ETC block diagram" in the ADC_ETC chapter.

jingpan_0-1677382059514.png

 

Regards,

Jing

0 Kudos