3 virtual com port on IMXRT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

3 virtual com port on IMXRT

1,424 Views
swaminathanrath
NXP Employee
NXP Employee

Hi,

I would like to enumerate 3 virtual com port device class on IMXRT1050 Board, do we have any example code?

Thanks & regards,

Swaminathan.R

Labels (1)
0 Kudos
Reply
2 Replies

1,298 Views
Sanjiv
Contributor II

Hello. Can this IP also be used on i.MXRT1010 CPU / EVK? Are there enough endpoints to build 3 CDC UARTs on the i.MXRT1010?

Thanks.

0 Kudos
Reply

1,298 Views
jia_guo
NXP Employee
NXP Employee

Add the code here.

0 Kudos
Reply