1176双核调试

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1176双核调试

695 Views
jingyangxie
Contributor V

IAR开发环境,是否有imxrt1176使用J-Link调试器双核调试的配置或方案,双核无关联同时调试测试是OK的,但想实现如官方Demo那样使用DAP调试,主核启动从核,同时调试方式(主核工程设置从核工程路径)

0 Kudos
4 Replies

679 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer the AN13264 [RT1170 Dual Core Application] Chapter 4.2 about IAR dual core debug.

Wish it helps.

Mike

0 Kudos

660 Views
jingyangxie
Contributor V

Hi,

I refer the AN13264 [RT1170 Dual Core Application] Chapter 4.2 about IAR dual core debug.but after the third step, the "attach the running target" label become gray and can not be clicked. like :

jingyangxie_0-1668746644748.png

and the m4 can not be debugged

0 Kudos

647 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi, I am using the IAR ARM V9.30.1, I am using below steps:

The steps for dual core debug by JLink are as below:

1. Build CM4 and CM7 projects.

2. Start CM7 debug session.

3. Run the CM7 project.

4. Run/Debug the CM4 project.

I also find the [Attach to Running Target] button is gray.

Thanks for the attention.

Hui_Ma_0-1669018487961.png

 

0 Kudos

644 Views
jingyangxie
Contributor V

Hi,

Looking forward to your updates.

Tags (1)
0 Kudos