flexspi_nor_sdram_debug\emwin_gui_demo.out: Error: L6218E: Undefined symbol Image$$RW_m_config_text$$Base (referred from fsl_flexspi_nor_boot.o).
这个问题是怎么造成的,需要怎么修改呢,谢谢
我也遇到了这问题,援引ZLG张工回复:
果然可以,真的是非常感谢
Hello,
Could you please provide more information regarding the problem you are facing? For example:
I'm using the latest version of the SDK (2.5.1) along with Keil 5.26.2 and I didn't face any problems with the emwin demo.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
I'm sorry to reply to you so late. I tested Standalone Example Project, not SDK.