Hi harry_liang,
非常好,我差不多知道你之前为什么不工作了。
你外挂的是TTL-USB啊?我还以为是什么debug工具呢?
话说,RT1020-EVK 板子就有串口,你为啥还要外挂串口?
你把你插的给扒了,然后把J9的USB也给拔掉。
就留USB接再J23, 你看看你电脑的设备管理器
这个串口号就是你板子的串口,然后你选择对应的串口, 同样在serial download模式,按下reset按键SW5.然后再连接:
你看我这边串口方式是不是也连成功了,你再试试。
Wish it helps you!
If you still have questions about it, please kindly let me know!
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hi harry_liang,
从你的提示看下来,说你引脚boot模式不对,你测试下你的引脚电平,到底是不是BOOT_MOD[1:0]=01?
你不用reset,你修改boot模式之后,重新上电试试,还有USB不要接了。就接TTL-USB 串口。
Wish it helps you!
If you still have questions about it, please kindly let me know!
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hi harry_liang,
你这是官方的板子啊,MIMXRT1020-EVK吗?
你把你外面的debugger给去了,直接用板载的USB 供电,然后你用USB HID试试。
还有,你把你MCUBootUtility的Boot device configuration发出来看看,你配制的对不对?
然后你再试试。
按道理,官方的板子,只要你没有乱修改fuse,还有硬件方面没有改把UART都给断开与RT的连接,不会连不上的。
如果是你自己的板子,我倒是要考虑是不是你硬件设计的不稳定导致的。
你再找个USB的线加上去,用USB HID试试,看看能不能成,按道理,进入serial download模式,你就能识别出USB HID的PID, VID了。
任何测试,请更新给我。
Best Regards,
Kerry
Hi harry_liang,
好的,如果你没乱操作过,我就放心了。你跟着我步骤走一遍,这个是最简单的操作了。
MCUBootutility工具前几天,作者又更新了一版,你也可以用最新版本,不过你这个版本也没有问题:
https://github.com/JayHeng/NXP-MCUBootUtility/archive/v2.4.0.zip
the related user manual is:
https://github.com/JayHeng/NXP-MCUBootUtility
你先断开所有连接:
1. SW8 1-OFF, 2-OFF, 3-OFF, 4-ON
我看你的照片是对的
2. 配置像我这样
3. 连接USB到J23,就是板载仿真器那边
4. 插入USB线到J9, 这个地方是USB HID, 按道理插入就可以识别USB了
5. 如果没有发现USB HID
你可以按下SW5,等个5-10s,看看是不是能识别了?
6 点击connect, 会发现连接成功
这个软件还有cmd的界面,你可以看到所有命令运行情况。
你再试下,看看是否能成功。
如果还有问题,还请告诉我。
Best Regards,
Kerry
Hi harry_liang,
非常好,我差不多知道你之前为什么不工作了。
你外挂的是TTL-USB啊?我还以为是什么debug工具呢?
话说,RT1020-EVK 板子就有串口,你为啥还要外挂串口?
你把你插的给扒了,然后把J9的USB也给拔掉。
就留USB接再J23, 你看看你电脑的设备管理器
这个串口号就是你板子的串口,然后你选择对应的串口, 同样在serial download模式,按下reset按键SW5.然后再连接:
你看我这边串口方式是不是也连成功了,你再试试。
Wish it helps you!
If you still have questions about it, please kindly let me know!
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hi harry_liang
板子硬件,其他地方动过没有?
看你现在这个情况,进入serialdownload模式之后,PID, VID都没认出来,说明你芯片压根就进不去serial download模式了,你之前修改过fuse为boot from fuse模式没有?
Wish it helps you!
If you still have questions about it, please kindly let me know!
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hi harry_liang,
楼主你好!
其实对于RT,烧录有很多种办法,你说的是IDE结合debugger去烧录。
这种情况下,通常是结合烧录算法以及你的app还有debugger去下载。
当然如果你自定义的flash loader,也放在flash的不同区域,通常是先下载flashloader,然后再去下载一个app。
如果你不想用这种分批下载,想一次性把你自定义已经在flash里面的flashloader还有app下载进去。
你还可以把两个文件合并成一个app,然后使用MFGTool,或者MCUBootUtility下载。
我认为,就算你是两个,你也可以用哪个MFGtool 去下载。其实就是在下载的时候,生成bd的情况下,要写下脚本,比如program_xxx.bd,然后把对应的文件吓到对应的区域即可了。
希望能帮到你,如果还有问题,欢迎继续交流!
Wish it helps you!
If you still have questions about it, please kindly let me know!
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------