关于sbl与sfw使用过程当中出现的问题

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

关于sbl与sfw使用过程当中出现的问题

跳至解决方案
3,114 次查看
944706426
Contributor III

按照文档MCUOTASBLSFWUG 中7.2.1部分  在powershell中read--memory命令中出错,这是啥原因

944706426_0-1649294442078.png

第一个命令get-property发完,板子一直在发 "hello sbl"

944706426_1-1649294583668.png

 

标签 (1)
0 项奖励
回复
1 解答
3,010 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

你试试使用MCU Boot Utility工具跟MCU进行交互,看看结果如何。

jeremyzhou_0-1651719645036.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
7 回复数
3,106 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

jeremyzhou_0-1649301940885.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
3,105 次查看
944706426
Contributor III

944706426_0-1649312238024.png

好像还是一样

0 项奖励
回复
3,093 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

请确认是否使能了SBL的MCU ISP?

jeremyzhou_0-1649324444067.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
3,029 次查看
944706426
Contributor III

还是那个问题

0 项奖励
回复
3,011 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

你试试使用MCU Boot Utility工具跟MCU进行交互,看看结果如何。

jeremyzhou_0-1651719645036.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
3,002 次查看
944706426
Contributor III
0 项奖励
回复
3,071 次查看
944706426
Contributor III

开启了的,返回结果是memory没有配置,不知道是啥情况

0 项奖励
回复