imxrt flashing error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxrt flashing error

1,163 Views
ancymuhammed
Contributor III

We are using MIMXRT1176AVM8A in our design. Initially the board was working. In between we are facing some failure issues in some of the boards. The screenshot of the error showing is shown below

ancymuhammed_0-1644414354678.png

ancymuhammed_1-1644414363105.png

 

ancymuhammed_2-1644414377359.png

We are using the frequency 1GHz and using internal DC-DC converters, external PMIC not used. 

0 Kudos
Reply
7 Replies

1,154 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I think I need more information about the issue, so I was wondering if you can introduce the testing environment, for instance, the schematic, debug tool, etc.
In further, what's the ratio of arising the issue?
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,148 Views
ancymuhammed
Contributor III

The below software and tool is used for programming.

MCUXpressoIDE – For programming via SWD

Tool used for programming– LPC-Link 2

 

Initially all boards are worked. After few days we are getting this fatilure. Out of 12 boards, 5 boards this failure seen

0 Kudos
Reply

1,108 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
Maybe you can try this trick to recover.
1) Set the MCU would enter to Serial Downloader.
2) Power on the board, debug the demo project.
3) After that, power off and recover MCU to the previous boot setting, then power on again.
4) Give a debug again.
Moreover, I was wondering if you can upload the schematic of your board.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply

1,104 Views
ancymuhammed
Contributor III

We had tried this option, but it didn't works. What may be the possible reason for this failure. Initially all boards are working fine. In between we are getting this issue. After replacing microcontroller it works for three times, after that same error is showing while flashing

0 Kudos
Reply

1,057 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
It seems a bit weird, whether you can share the schematic of the customize board.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,141 Views
ancymuhammed
Contributor III

We had replaced the microcontroller in one board. Initially it was working, but after some time the same error is showing during programming. But the controller is still working with the old flashed code. 

0 Kudos
Reply

644 Views
eRgnmrt
Contributor III
Hi
Was the application that you used internal dc dc as 1 ghz for automotive?
0 Kudos
Reply