iMXRT1052 LCD Drive Capacity

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMXRT1052 LCD Drive Capacity

742 次查看
kohama
Contributor I

I want to drive a 1280x800 pixel LCD at 60Hz on the iMXRT1052.
Is it possible?
If possible, please provide example parameters.

标签 (1)
0 项奖励
回复
2 回复数

635 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Toru,

 

I recommend to check the following community post.

 

IMX RT1050 LCD Resolution 

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

635 次查看
kohama
Contributor I

Thank your advice.
I'll ask a question to other community post.

0 项奖励
回复