Hello,
On a board, I have an iMXRT1052 or iMXRT1062 (pin to pin compatible) with ethernet in RGMII (ENET_RX_DATA0/DATA1, ENET_TX_DATA0/DATA1), and I need to add an LCD. I have check on datasheet and it seems like only 16bpp is possible.
Can you confirm that it is possible to have an RGB bus in 24bpp for the LCD or only 16bpp will be possible?
Thanks
Hello, David
According to the datasheet section 1.1, the parallel RGB LCD interface supports 8/16/24 bit interface.
Have a great day,
Victor
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Yes thank you Victor,
I know that 24bpp is possible, my question is :24 bpp possible with ethernet in RGMII (ENET_RX_DATA0/DATA1, ENET_TX_DATA0/DATA1) or only 16bpp will be possible since the pins of ENET are shared with LCD? Or in other words, is it possible to have 24bpp LCD and remap the ENET signals on other pins in order to have both functions working at the same time?
Regards
Hello, David
Thanks for clarifying, which pins are the ones you find conflicts?
Regards,
Victor