iMXRT1050 - When to use FLEXSPI_1PAD/FLEXSPI_2PADS/FLEXSPI_4PADS/FLEXSPI_8PADS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMXRT1050 - When to use FLEXSPI_1PAD/FLEXSPI_2PADS/FLEXSPI_4PADS/FLEXSPI_8PADS

ソリューションへジャンプ
1,018件の閲覧回数
Cindy
Contributor III

Hi,

For FLEXSPI, there are these pad options to select:-

kSerialFlash_1Pad = 1,
kSerialFlash_2Pads = 2,
kSerialFlash_4Pads = 4,
kSerialFlash_8Pads = 8,

 

How do I know  when to select 1Pad/2Pads/4Pads/8Pads.

What are the meanings/definitions for each of the pad options?

 

For example, const flexspi_nor_config_t qspiflash_config = {
.memConfig =
{
.tag = FLEXSPI_CFG_BLK_TAG,
.version = FLEXSPI_CFG_BLK_VERSION,
.readSampleClksrc=kFlexSPIReadSampleClk_LoopbackFromDqsPad,
.csHoldTime = 3u,
.csSetupTime = 3u,
// Enable DDR mode, Wordaddassable, Safe configuration, Differential clock
.sflashPadType = kSerialFlash_4Pads,
.serialClkFreq = kFlexSpiSerialClk_100MHz,
.sflashA1Size = 8u * 1024u * 1024u,
.lookupTable =
{
// Read LUTs
FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x18),
FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, 0x06, READ_SDR, FLEXSPI_4PAD, 0x04),
},
},
.pageSize = 256u,
.sectorSize = 4u * 1024u,
.blockSize = 256u * 1024u,
//.isUniformBlockSize = false
};

 

What is the impact of setting sflashPadType to kSerialFlash_4Pads?

.sflashPadType = kSerialFlash_4Pads,

 

If I change the line to

.sflashPadType = kSerialFlash_2Pads,

What will happen?

 

Please explain.Thank you!

 

Best Regards,

Cindy

 

 

0 件の賞賛
返信
1 解決策
1,012件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Cindy ,

   My PPT page will help you:

kerryzhou_0-1656991805200.png

In fact, it  is related to your used flash, check my above picture.

You will find your code related command, fast read:

// Read LUTs
FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x18),
FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, 0x06, READ_SDR, FLEXSPI_4PAD, 0x04),

0XEB -> fast read command, 1 wire, so use FLEXSPI_1PAD

0X18 ->3 Byte address, 3*8=24bit=0x18, but you can see 3 bytes address is 4 wire, so, it use FLEXSPI_4PAD.

0X06 -> DUMMY cycle, 4 pad, so use FLEXSPI_4PAD.

0X04->4 bytes read out, with 4 pad, so use FLEXSPI_4PAD.

 

Wish my picture and description helps your understanding.

Best Regards,

kerry

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,013件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Cindy ,

   My PPT page will help you:

kerryzhou_0-1656991805200.png

In fact, it  is related to your used flash, check my above picture.

You will find your code related command, fast read:

// Read LUTs
FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x18),
FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, 0x06, READ_SDR, FLEXSPI_4PAD, 0x04),

0XEB -> fast read command, 1 wire, so use FLEXSPI_1PAD

0X18 ->3 Byte address, 3*8=24bit=0x18, but you can see 3 bytes address is 4 wire, so, it use FLEXSPI_4PAD.

0X06 -> DUMMY cycle, 4 pad, so use FLEXSPI_4PAD.

0X04->4 bytes read out, with 4 pad, so use FLEXSPI_4PAD.

 

Wish my picture and description helps your understanding.

Best Regards,

kerry

 

 

0 件の賞賛
返信
982件の閲覧回数
Cindy
Contributor III

Hi KerryZhou,

 

Your pic and description have been very helpful! Thank you!

 

Best Regards,

Cindy

0 件の賞賛
返信