iMX RT685 EVK Debug failed with SIGTRAP when using JLink Firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX RT685 EVK Debug failed with SIGTRAP when using JLink Firmware

1,535 Views
yugandhar421
Contributor II

Hi,

I was able to debug few sample apps of iMX RT685 with onboard LPC Link as LinkServer debug probe and code downloaded to RAM.

Now I want to test few DSP sample apps, so I programmed latest JLink firmware to onboard LPC Link then it detected as SEGGER JLink probe. But when I try to debug any app, received SIGTRAP.

 

Below is the version info.

MCUXpresso IDE v11.3.0 [Build 5222] [2021-01-11]

Firmware_JLink_LPCXpressoV2_20190404.bin

 

I verified few other posts related to SIGTRAP, but no one solved my problem. If any one has ideas please share.

 

Thanks,

Yugandhar

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

1,522 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @yugandhar421,

In the following post is explained how to update the onboard LPC-Link. Did you replace the LPC-link image?

Best Regards,

Alexis Andalon

0 Kudos
Reply

1,520 Views
yugandhar421
Contributor II

Hello @Alexis_A 

 

Yes, I flashed Firmware_JLink_LPCXpressoV2_20190404.bin then it detected as JLink.

0 Kudos
Reply

1,498 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @yugandhar421,

In the following link you can download the user manual of the EVK, could you check the default state of the jumpers and see if them match with your board?

Also, only to confirm the LPC link Firmware is the following one?

Alexis_A_0-1623081787502.png

 

Best Regards,

Alexis Andalon

0 Kudos
Reply