iMX RT1050 24MHz clock signal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX RT1050 24MHz clock signal

1,562 Views
davidouatt08
Contributor I

Hello,

On a project, I need to generate the 24MHz XTALi signal from an external oscillator which outputs 1.8V signals.

To meet the requirement of the iMXRT1052, I use a capacitive voltage divider but the signal out of the divider is below 0V (see attached picture) specified in the IMXRT1050IEC document, page 31.

The High level is also to close to Vihmin. 

A resistive voltage divider modifies the signal too much.

What is the best way to do this voltage division in order to meet the NXP requirements?

Regards 

Labels (2)
0 Kudos
Reply
1 Reply

1,367 Views
jeremyzhou
NXP Employee
NXP Employee

Hi David OUATTARA,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Please refer to the below figure to optimize the voltage divider, and note that: don't use the large resistors (> 300Ω) in the voltage divider.

pastedImage_1.png
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply