iMX RT1020 EVK SEMC-ENET pin rounting collision

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX RT1020 EVK SEMC-ENET pin rounting collision

395 Views
ByoungogCho
Contributor I

iMX RT1020EVK - MIMXRT1021DAG5A  question,

In. SDK  SDRAM example,    csx,0 & RDY pin at Rouning Details,  is below

ByoungogCho_0-1690516775067.png

In SDK tcp/ip example,   MDIO & MDC pin  at Rouning Details, is below.   and  it use  same gpio pin

ByoungogCho_1-1690516884580.png   mdio in/out  pin , mdc  is out pin

So. I checked the schemetics of 1020EVK board. and Hardware Development Guide  app.note

curiously,  In schemetics,    GPIO_EMC_40,GPIO_EMC_41 pins connected only with  ENET part,  and  I can not find any connection  SEMC 2 pin (csx0, rdy)

ByoungogCho_2-1690517346985.png   mdio out  pin , mdc  is In/out pin  (??)

In this schemetics,   pin direction is also not same  with tcp/ip example routing, what is wrong?

 

I have to use SDRAM and Ethernet,   csx,0 & RDY for SEMC(forSDRAM)  no need to rout also in software?  then  what is the purpose of this csx0, RDY ? why In exameple this two pins are routed? 

 

and If  I connect 116,115 pins  to  ENET_MDIO,MDC ,   according to direction,  which configuration of direction is  Ok ?

If  I  do  rout  like this,  (ENET_MDIO,MDC - 115,116 ) ,(csx,0 & RDY  - 91,92 (another routable pins) ),

,   but... 91, 92 pin is also connected to  WM8960,  SAI1_MCLK,  SAI1_TX_BCLK in schemetics of board

Please Let me know. 

 

0 Kudos
Reply
1 Reply

367 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

If you are using one SDRAM then RDY and CSX0 are unused. CSX signal is used for chip select if another SDRAM/memory is used while RDY is for NAND memory.

Omar_Anguiano_0-1690834297023.png

 

Best regards,
Omar

0 Kudos
Reply