i.mx rt1050 example flexspi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx rt1050 example flexspi

3,872件の閲覧回数
christiangradl
Contributor III

Hi

i did some speed tests, using "FLEXSPI hyperflash example" and my EVK board.

in the example at line 500 i found the comment

/* flexspi clock 332M, DDR mode, internal clock 166M. */

and the following code line

memcpy(s_hyperflash_read_buffer, (void *)(FlexSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE), sizeof(s_hyperflash_read_buffer));

i put my LED_on(), LED_Off() macros berofe and after this memcpy function

and started my measurements.

this memcpy (512 Byte from QSPI)  needs about about 34.8 us, thats very slow for the "fast" 166MHz QSPI.

I expected following: 166 Mhz for QSPI  => 332 MHz in DDR mode and 512 Byte Data and adding some overhead data (QSPI cmd, addr, etc.) => 2 us!!!

How can i speed the communication?

ラベル(1)
0 件の賞賛
返信
9 返答(返信)

2,679件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

When trying to understand the read behaviour from Flash, please remember that this is a cached MCU - where a hit in the cache will not of course perform a flash access at all. Any read will first check the cache contents, only if a miss occurs will the a sequence begin to perform a read.

I suggest taking a look at the User Manual for this part, specifically 'AHB read access to Flash' to better understand what is occurring.

Yours,

MCUXpresso IDE Support

0 件の賞賛
返信

2,679件の閲覧回数
rans
Senior Contributor I

Hello,

I hope someone can help me understanding the following:

In hyperflash examples, Is it that reading is done by pointer de-reference (like memcpy), but writing done through specific driver (can't use dereference for writing) ?

Thank you,

ranran

0 件の賞賛
返信

2,679件の閲覧回数
christiangradl
Contributor III

hi

i check the clock settings

    CLOCK_InitUsb1Pfd(kCLOCK_Pfd0, 26);   /* Set PLL3 PFD0 clock 332MHZ. */

    CLOCK_DisableClock(EXAMPLE_FLEXSPI_CLOCK);
    CLOCK_SetDiv(kCLOCK_FlexspiDiv, 0); /* flexspi clock 332M, DDR mode, internal clock 166M. */
    CLOCK_EnableClock(EXAMPLE_FLEXSPI_CLOCK);
    FLEXSPI_Enable(EXAMPLE_FLEXSPI, true);

    i = CLOCK_GetFreq(kCLOCK_Usb1PllPfd0Clk);
    PRINTF("PFD Clock=%lu \r\n", i);
    i = CLOCK_GetFreq(kCLOCK_Usb1PllPfd0Clk) / (CLOCK_GetDiv(kCLOCK_FlexspiDiv) + 1U);
    PRINTF("With Div=%lu \r\n", i);

=> Output from the example project

FLEXSPI hyperflash example started!
Entering the ASO mode
Found the HyperFlash by CFI
Erasing Serial NOR over FlexSPI...
Erase data - successfully.
PFD Clock=332307684
With Div=332307684
Program data - successfully.

0 件の賞賛
返信

2,679件の閲覧回数
christiangradl
Contributor III

hi,

what do mean with

1.) "additional delays happen"

--------------------------------------

   the code is in itcm, i also checked the code with IDA (Interactive Disassembler) there are no "delays". memcpy is in itcm

Here the asm code

MENK_Run:
   ER_m_text:000034FE                 LDR             R0, =0x401B8000
   ER_m_text:00003500                 LDR             R0, [R0]
   ER_m_text:00003502                 BIC.W           R0, R0, #0x400
   ER_m_text:00003506                 LDR             R1, =0x401B8000
   ER_m_text:00003508                 STR             R0, [R1]
   ER_m_text:0000350A                 ASRS            R2, R1, #0x15
   ER_m_text:0000350C                 LDR             R1, =0x61940000
   ER_m_text:0000350E                 LDR             R0, =menk_read_buffer
   ER_m_text:00003510                 BL              __aeabi_memcpy8
   ER_m_text:00003514                 LDR             R0, =0x401B8000
   ER_m_text:00003516                 LDR             R0, [R0]
   ER_m_text:00003518                 ORR.W           R0, R0, #0x400
   ER_m_text:0000351C                 LDR             R1, =0x401B8000
   ER_m_text:0000351E                 STR             R0, [R1]

__aeabi_memcpy8:
   ER_m_text:00000694                 EXPORT __aeabi_memcpy8
   ER_m_text:00000694 __aeabi_memcpy8
   ER_m_text:00000694  .............

      There is no delay,

2.) "and used flexspi clock frequency"

------------------------------------------------

0 件の賞賛
返信

2,679件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

"   Here the asm code

There is no delay, "

actually these asm codes consume some processor time and introduce delays,

they may be observed with oscilloscope.

Also may be useful to check clocks using sect.2.3. FlexRAM module-related clocks and clock gates

AN12077 Using the i.MX RT FlexRAM

https://www.nxp.com/docs/en/application-note/AN12077.pdf 

0 件の賞賛
返信

2,679件の閲覧回数
christiangradl
Contributor III

hi,

the code (example code from NXP) is running in ICTM and needs 9,4 us for 512 Byte

/* flexspi clock 332M, DDR mode, internal clock 166M. */

memcpy(s_hyperflash_read_buffer, (void *)(FlexSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE), sizeof(s_hyperflash_read_buffer));

the memcpy  uses ldmia and stmia asm instruction => ca. 128 (loads + stores + sub + cmp + brunch) => 128 * 5 instructions => 640 instructions

the cpu is running with 600 mhz.

so you think these 640 instructions needs more than 7 us?

not really. 640 instructions => ~1 us but not 7 us

i am using the example project that says 332M DDR mode.

0 件の賞賛
返信

2,679件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Christian

for better results recommended not to use debug mode and run image

from ITCM.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,679件の閲覧回数
christiangradl
Contributor III

Hi

i tried this already, i moved the important copy code to a separate c-file

void Testcopy(void)

{

   __disable_irq();
   DEBUGLED_On();
   memcpy(menk_read_buffer, (void *)(FlexSPI_AMBA_BASE + 101 * SECTOR_SIZE), sizeof(menk_read_buffer));
   DEBUGLED_Off();

   __enable_irq();

}

and made changes to the scatter file. 

The Testcopy function is in ICTM, my testbuffer is in ocm, etc. etc.

i checked the map file.

so the thing is, has anyone checked the speed with 332 mhz?

what are the right settings?

do you have an example code, that copies 512 byte in 2 us, as expected?

0 件の賞賛
返信

2,679件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

you can check with oscilloscope where additional delays happen

and used flexspi clock frequency.

Best regards
igor

0 件の賞賛
返信