Hello,
I have a question regarding the LPSPI of the i.MXRT1166:
The i.MX RT1160 Reference Manual Rev. 0 05/2021 describes the HRSEL, HRPOL and HREN bits in the LPSPI CFGR0. There is a note at the beginning of the LPSPI chapter that 'The "Output Triggers" section is not applicable for this device.' The HREQ is an input trigger so I would expect that the note is not relevant.
But at the same time the header file for the i.MXRT1166 in the mcux-sdk doesn't define the HRSEL, HRPOL and HREN bits: https://github.com/nxp-mcuxpresso/mcux-sdk/blob/main/devices/MIMXRT1166/MIMXRT1166_cm7.h
That makes me a bit suspicious: Does the i.MXRT1166 LPSPI support HREQ or is that feature missing?
With kind regards
Christian Mauderer
已解决! 转到解答。
HREQ is supported on the RT11xx devices. The absence of the HRSEL, HRPOL and HREN bits on the core's header file is most likely a bug. I will report this to the SDK team to deliberate about this issue and make the appropriate changes.
BR,
Edwin.
HREQ is supported on the RT11xx devices. The absence of the HRSEL, HRPOL and HREN bits on the core's header file is most likely a bug. I will report this to the SDK team to deliberate about this issue and make the appropriate changes.
BR,
Edwin.