i.MX RT1170 External 3 SRAM devices usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1170 External 3 SRAM devices usage

Jump to solution
478 Views
Eugene3
Contributor II

I'd like to use 3 external SRAM interface devices on RT1170 SEMC bus.

Each device has different access timing.

 

In the spec, RT1170 can have only 2 configuration tables for SRAM0 and SRAM1-3.

Is there any way to have third configuration table? 

Is it possible to use nor flash config table for SRAM device access?

 

 

 

0 Kudos
Reply
1 Solution
433 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Eugene3 ,

 

It is due to the chip spec, no third configuration table available for SRAM , and it is not possible to use nor flash config table for SRAM device access either.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
434 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Eugene3 ,

 

It is due to the chip spec, no third configuration table available for SRAM , and it is not possible to use nor flash config table for SRAM device access either.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply