eLCDIF controller for iMXRT1060

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eLCDIF controller for iMXRT1060

611 Views
EmbeddedTech
Contributor III

Hi, 

We are planning to use the 7" parallel RGB display from EDT with the iMXRT1060.

part number of EDT display is ETML070017ADH6.

For pin connection to the MCU, there is a pin called MODE to select DE or SYNC.

We are not clear what mode should be used for the eLCDIF controller.

Your help on this is highly appreciated.

Thanks.

0 Kudos
Reply
3 Replies

578 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @EmbeddedTech ,

I couldn't find the spec of ETML070017ADH6. But here I think you can only use SYNC mode which has VSYNC/HSYNC/DE.

 

Regards,

Jing 

0 Kudos
Reply

556 Views
EmbeddedTech
Contributor III

Hi,

So only displays which support Sync mode can be used with this controller right?

Thanks

0 Kudos
Reply

527 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @EmbeddedTech ,

Yes.

 

Regards,

Jing

0 Kudos
Reply