eLCDIF controller for iMXRT1060

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eLCDIF controller for iMXRT1060

615 次查看
EmbeddedTech
Contributor III

Hi, 

We are planning to use the 7" parallel RGB display from EDT with the iMXRT1060.

part number of EDT display is ETML070017ADH6.

For pin connection to the MCU, there is a pin called MODE to select DE or SYNC.

We are not clear what mode should be used for the eLCDIF controller.

Your help on this is highly appreciated.

Thanks.

0 项奖励
回复
3 回复数

582 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @EmbeddedTech ,

I couldn't find the spec of ETML070017ADH6. But here I think you can only use SYNC mode which has VSYNC/HSYNC/DE.

 

Regards,

Jing 

0 项奖励
回复

560 次查看
EmbeddedTech
Contributor III

Hi,

So only displays which support Sync mode can be used with this controller right?

Thanks

0 项奖励
回复

531 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @EmbeddedTech ,

Yes.

 

Regards,

Jing

0 项奖励
回复