blhost to write RT1015 GPIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

blhost to write RT1015 GPIO

Jump to solution
699 Views
kensu
Contributor V

Hi 

I want to control RT1015 GPIO in download mode,

Is it possible?

I read the user manual, it look like it can.

4.2.8 write-memory <addr> [<file> | {{<hex-data>}}][memoryID]

 pastedImage_1.png

And what is “minimum profile”?

Regards

Ken

Labels (1)
Tags (2)
1 Solution
641 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ken Su

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
1) Is it possible?
-- I think it's possible, you can give a try.
2) what is “minimum profile”?
-- The writing byte sizes should be a multiple of word-size.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
642 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ken Su

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
1) Is it possible?
-- I think it's possible, you can give a try.
2) what is “minimum profile”?
-- The writing byte sizes should be a multiple of word-size.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------