Unable to debug on IMXRT1050-EVKB (0 available SWD Devices detected).

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to debug on IMXRT1050-EVKB (0 available SWD Devices detected).

Jump to solution
10,581 Views
Murtn
Contributor II

I'm trying to debug an example project on a IMXRT1050-EVKB using MCUXpresso IDE. I've imported SDK example "evkbimxrt1050_iled_blinky" built it and tried to debug it. 

When starting the debugging I get prompted with a message saying:

SWD Configuration. 0 available SWD Devices detected.

How can I resolve this problem?

Kind regards,

 

 

Labels (1)
0 Kudos
Reply
1 Solution
10,561 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the attachment for it which is similar with the RT1050.

Hope it help you. Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

View solution in original post

6 Replies
9,352 Views
expertsleepers
Contributor III

Does anyone actually know how to stop the boards getting into this situation in the first place? Having to constantly use the Boot Utility to recover is not sustainable.

 

0 Kudos
Reply
9,571 Views
ejd037
Contributor I

It would be great if one of the moderators would put recover_rt1064.pdf, and the like, on all Get Started pages for the EVK boards. Took me most of the day to stumble on this. Thanks again to "fangfang" for posting it.

0 Kudos
Reply
10,359 Views
andy4
Contributor I

This worked for the MIXRT1060-EVK board when it had the "0 available SWD Devices" message as well.

10,562 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the attachment for it which is similar with the RT1050.

Hope it help you. Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

9,276 Views
bloom11
Contributor II

Thanks, this PDF that you shared, explaining the process to access the recovery mode of the board/MCU work fine on the 1060(tested)/1064(tested)/1062 and maybe 1050 from the different comments i have seen. It has been really useful in my case and save me a lot of time.

0 Kudos
Reply
10,555 Views
Murtn
Contributor II

This seemed to do the trick.

Thank you!

0 Kudos
Reply