Hi all,
I am trying to use the USB as a device on port J10 instead of J9 on the MXRT1064-evk. I am using the dev_cdc_vcom_lite_bm example in SDK_2.4.1_EVK-MIMXRT1064 and IAR. I did find this post from a while ago https://community.nxp.com/thread/492145, but I am not having any luck. In virtual_com.h I have changed:
#define CONTROLLER_ID kUSB_ControllerEhci0
to
#define CONTROLLER_ID kUSB_ControllerEhci1
What else needs to be done to change the device id?
解決済! 解決策の投稿を見る。
Hi Heath Pritchett
Currently, there are no platforms which have two EHCI IPs, so, when you defined kUSB_ControllerEhci1 it gives an error as "ControllerNotFound". RT1050 already uses SDK v2.5 (while RT1064 uses 2.4.1) and it has implemented differently the usb_ehci driver, so you can tell the driver to use the USBOTG2 with the software of the EHCI device.
Until the SDK driver is updated to 2.5, as a workaround you could use the following code in the usb/device/source/ehci/usb_device_ehci.c file.
............... if ((controllerId < kUSB_ControllerEhci0) || // ((uint32_t)(controllerId - kUSB_ControllerEhci0) >= USB_DEVICE_CONFIG_EHCI) || ((uint32_t)(controllerId - kUSB_ControllerEhci0) >= (sizeof(ehci_base) / sizeof(uint32_t)))) { return kStatus_USB_ControllerNotFound; } ehciState = &g_UsbDeviceEhciSate[controllerId - kUSB_ControllerEhci0 - 1]; ehciState->dtd = s_UsbDeviceEhciDtd[controllerId - kUSB_ControllerEhci0 -1 ]; ehciState->qh = (usb_device_ehci_qh_struct_t *)&qh_buffer[(controllerId - kUSB_ControllerEhci0 - 1) * 2048]; ehciState->controllerId = controllerId; .................
Hope this helps
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------
Hi Heath Pritchett
Currently, there are no platforms which have two EHCI IPs, so, when you defined kUSB_ControllerEhci1 it gives an error as "ControllerNotFound". RT1050 already uses SDK v2.5 (while RT1064 uses 2.4.1) and it has implemented differently the usb_ehci driver, so you can tell the driver to use the USBOTG2 with the software of the EHCI device.
Until the SDK driver is updated to 2.5, as a workaround you could use the following code in the usb/device/source/ehci/usb_device_ehci.c file.
............... if ((controllerId < kUSB_ControllerEhci0) || // ((uint32_t)(controllerId - kUSB_ControllerEhci0) >= USB_DEVICE_CONFIG_EHCI) || ((uint32_t)(controllerId - kUSB_ControllerEhci0) >= (sizeof(ehci_base) / sizeof(uint32_t)))) { return kStatus_USB_ControllerNotFound; } ehciState = &g_UsbDeviceEhciSate[controllerId - kUSB_ControllerEhci0 - 1]; ehciState->dtd = s_UsbDeviceEhciDtd[controllerId - kUSB_ControllerEhci0 -1 ]; ehciState->qh = (usb_device_ehci_qh_struct_t *)&qh_buffer[(controllerId - kUSB_ControllerEhci0 - 1) * 2048]; ehciState->controllerId = controllerId; .................
Hope this helps
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------