Hello,
I try to use semohist (vrtual com) with fsl_debug_console.h:
#define SDK_DEBUGCONSOLE 0U
#define _SDK_DEBUGCONSOLE_UART
But it only works with baremetal, with freertos, the thread is keep waiting on fgetc().
Is there a way to overcome this ?
Thanks,
ranran
Hi ranran,
What the RT board you are using? Do you try the SDK code freertos sample code directly?
What's the IDE you are using now? I will help you to check it .
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
>What the RT board you are using?
imxRT1050
>Do you try the SDK code freertos sample code directly?
Yes, can this code works with both freertos+semihost (instead of uart), or is it that semihost can only be done with baremetal ?
I have changed in fsl_debug_console.h to: (maybe this is not the correct changes that should be done?)
#define SDK_DEBUGCONSOLE 0U
#define _SDK_DEBUGCONSOLE_UART
> What's the IDE you are using now?
IAR
Thank you very much for any idea,
ranran
Hi ranshalit,
As I know, the MCUXpresso IDE project can select it to semihost or UART directly.
So, do you mind to try the MCUXPresso project?
You can find it can printf to the console directly.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Kerry,
Thank yo very much for the help!
I understand that the project (with freeRTOS) demonstrate "printf".
Yet, the big question is if it can also use fgetc (wait for a character input), while still are threads are keep running ?
Thanks,
ranran
Hi ranran,
You can create a new task, then use the GETCHAR.
static void hello_task(void *pvParameters)
{
char ch;
for (;;)
{
// PRINTF("Hello world.\r\n");
// vTaskSuspend(NULL);
ch = GETCHAR();
PUTCHAR(ch);
}
}
Wish it helps you!
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello Kerry,
I think it won't work becuase GETCHAR is fgetc, which is non blocking, and is sory of busy wait, without freeing the thread to any other running threads.
Did you try it ?
Thanks,
ranran
Hi ranran,
I think you totally can try it on your side at first, if you want to add any other task.
And, it is freertos usage now, not the RT chip question.
At least, if I try one task, it works OK.
You can test it, if you still have any other question, you can post the freertos question and let us know, thank you!
Have a great day,
kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------