[Samsung/Bixby Module/iMXRT1020] Image Download

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[Samsung/Bixby Module/iMXRT1020] Image Download

1,734 次查看
Harrison_Choi
NXP Employee
NXP Employee

Hello

I am currently supporting TIZEN RT only used in Samsung for their own RTOS.

In the current status, I copy the hex format binary to RT1050-EVK folder that is automatically decteded when image update.

But the fail to download image often happens.

In that case, fail.txt file is shown in RT1050-EVK folder and image download didn't work well.

Please give me the guidance about image download without IAR or MCU Expresso.

or share the external image tool to download built image.

Thanks

标签 (1)
0 项奖励
回复
7 回复数

1,587 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Harrison Choi ,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
In the application note: AN12108, it illustrates the steps of programming the boot image to external flash, in further, the NXP-MCUBootUtility is a GUI tool specially designed for NXP MCU secure boot, Its features correspond to the BootROM function in NXP MCU. Currently, it mainly supports i.MXRT series MCU chips and please go to download it, then give a try.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,587 次查看
Harrison_Choi
NXP Employee
NXP Employee

Hello Jeremyzhou

Please tell me how to get the execution file..

I cannot execute NXP-MCUBootUtility.exe file in Windows10 OS

Best Regards

Harrison

0 项奖励
回复

1,587 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Harrison Choi,

Thanks for your reply.
Whether you can tell me what error you encountered.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,587 次查看
Harrison_Choi
NXP Employee
NXP Employee

Hello

I met this problem whenever I execute the above program named NXP-MCUBootUtility.exe

pastedImage_1.png

Please check it at your earliest convenient time

0 项奖励
回复

1,587 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Harrison Choi,

It seems a bit weird, the tool works well in my PC (Win10 64 bit).
The NXP-MCUBootUtility.exe in the source code package is packaged in the Windows 10 x64 environment, thus it should work well in the Win10.
Whether you try other PC for testing.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,587 次查看
Harrison_Choi
NXP Employee
NXP Employee

Hello

Please share your execution file by attaching this thread.

I want to check yours.

Best Regards

Harrison

0 项奖励
回复

1,587 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Harrison Choi,

Thank you for your reply.
You can download the NXP-MCUBootUtility-master via the link: NXP-MCUBootUtility-master.zip - Google Drive 
It works well on my laptop.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复