SNVS general purpose registers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SNVS general purpose registers

ソリューションへジャンプ
1,822件の閲覧回数
DanielePagani
Contributor II

    Dear sirs,

we're wondering if it's correct to use the SNVS module for temporary storage of some variables, in order to keep their value even after a Reset Software. 

As example:

#include "fsl_snvs_lp.h"

int main(void){

...

uint32_t registers[4];

SNVS_LP_Init(SNVS);

registers[0]=SNVS->LPGPR_ALIAS[0];

registers[1]=SNVS->LPGPR_ALIAS[1];

registers[2]=SNVS->LPGPR_ALIAS[2];

registers[3]=SNVS->LPGPR_ALIAS[3];

PRINTF("Registers:%u,%u,%u,%u\n",registers[0],registers[1],registers[2],registers[3]);

registers[0]++;

registers[1]+=2;

registers[2]+=3;

registers[3]+=4;

SNVS->LPGPR_ALIAS[0]=registers[0];

SNVS->LPGPR_ALIAS[1]=registers[1];

SNVS->LPGPR_ALIAS[2]=registers[2];

SNVS->LPGPR_ALIAS[3]=registers[3];

SNVS_LP_Deinit(SNVS);

NVIC_SystemReset();

...

}

The example seems to work fine, but at Chapter 19.2 - SNVS introduction of IMXRT1060 Reference Manual (we're using MIMXRT1060-EVK board) we read:

"SNVS incorporates both security and non-security functionality. The SNVS non-security functionality is described in this document, but the SNVS security functionality is described only in the Security Reference Manual."

We don't know if some security-related features can affect general purpose registers.

BR

Daniele

ラベル(1)
0 件の賞賛
返信
1 解決策
1,638件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Daniele,


If I understood correctly, you want to use the SNVS_LP General Purpose Registers, right? If this is the case, then the security features won't affect these registers at all.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,639件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Daniele,


If I understood correctly, you want to use the SNVS_LP General Purpose Registers, right? If this is the case, then the security features won't affect these registers at all.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信