Dear NXP Support Team,
I have a couple of questions regarding the boot configuration settings for our project:
I have attached images for your reference. Please update me as soon as possible.
Your assistance in clarifying these points would be greatly appreciated.
I appreciate your support.
Best regards,
Sagar
Solved! Go to Solution.
If using boot from fuses then the boot_cfg pins can be used for other purpose as the ROM will read the values from the fuses instead of the GPIOs.
The state of the pins can be as a normal pin as the state of the GPIO will not be read on that mode.
Best regards,
Omar
If using boot from fuses then the boot_cfg pins can be used for other purpose as the ROM will read the values from the fuses instead of the GPIOs.
The state of the pins can be as a normal pin as the state of the GPIO will not be read on that mode.
Best regards,
Omar
Hello @Omar_Anguiano ,
Thank you for the quick reply.
I have another query: if we use Boot from Fuses, can we change it later if we want to?
Is Serial Downloader and Internal Boot compulsory? If we set the fuses, can we change the fuse settings afterward?
In the reference design file, it is mentioned that the Boot Mode selection header should be used only during the development phase. We use Boot Selection settings during the development phase, but after finalizing the production phase, we switch to Boot from Fuses. What happens if we want to change the bootloader and firmware again after setting Boot from Fuses?
Thanks
Sagar