Reallocating the flexRAM for MIMXRT1062

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reallocating the flexRAM for MIMXRT1062

588 Views
yalin_10
Contributor II

Hi 

I am working on the MIMXRT1062. 

The SRAM_DTC is overflowed "SRAM_DTC". I tried to double the SRAM_DTC to 256KB and decrease the SRAM_OC accordingly(below). After that, the debugger stops working.

I have already tried this way - link 

1. How to reallocate FlexRAM for MIMXRT1062.

Labels (1)
0 Kudos
Reply
3 Replies

580 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @yalin_10 ,

  Which IDE and debugger you are using now?

  Which situation following you are using?

kerryzhou_0-1685002487265.png

You may select item 8, or 9.

If you use the mcuxpresso IDE and CMSIS DAP, you also need to modify the script file for the debugger with the reallocated flexRAM configuration.

 

Best Regards,

Kerry

 

0 Kudos
Reply

559 Views
yalin_10
Contributor II

Hi @kerryzhou 

After following the below mentioned procedure, board isn't responding, I changed those register values using NXPBootUtility

 

0 Kudos
Reply

533 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @yalin_10 ,

  Do you mean MCUbootutility?

  As you change the fuse for the reallocation? You didn't change the register with code? Then you boot from fuse?

 

Best Regards,

Kerry

0 Kudos
Reply