RT595 max UART baud rate

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT595 max UART baud rate

647 次查看
dpoulsen
Contributor I
The datasheet states that the UARTS are functional up to 20 Mbit/s in synchronous mode, but when configured as a UART, they can only run up to 921600 bps (found in the Baud Rate Generator section)?
 
 
dpoulsen_1-1667576581839.png 
 
Am I reading that correctly?
I want to run the UART at 4Mbit, with the Flexcomm clock at 48 MHz and the oversampling at 12x. Is this feasible?
0 项奖励
回复
1 回复

620 次查看
jeremyzhou
NXP Employee
NXP Employee


Hi @dpoulsen ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Is this feasible?
-- Yes, I think so.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the

0 项奖励
回复