RT117x: where is the FORCE_COLD_BOOT fuse reflected?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT117x: where is the FORCE_COLD_BOOT fuse reflected?

Jump to solution
1,062 Views
mastupristi
Senior Contributor I

On the Ref Man I read:

Screenshot_2023-04-11_18-15-01.png

the FORCE_COLD_BOOT should be reflected in SRC_SBMR...

I looked for SRC_SBMR and found two registers, but in neither of them do I seem to see the bit reflected by the FORCE_COLD_BOOT fuse.

Could you point me to which register and which bit I find it in?

best regards

Max

Tags (3)
0 Kudos
Reply
1 Solution
1,039 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

This is true. Confirmed by support engineer.

 

Regards,

View solution in original post

0 Kudos
Reply
4 Replies
1,046 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

For RT1170, I think this fuse bit is not touched by ROM. You can ignore it.

 

Regards,

Jing

0 Kudos
Reply
1,042 Views
mastupristi
Senior Contributor I

I think this fuse bit is not touched by ROM. You can ignore it.

Is this your feeling or do you have written confirmation in some document?
Because the only document I have available says the fuse is there and it's reflected somewhere on SRC.

 

best regards

0 Kudos
Reply
1,040 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

This is true. Confirmed by support engineer.

 

Regards,

0 Kudos
Reply
1,037 Views
mastupristi
Senior Contributor I

Then I suggest removing the description of that fuse from both the Refernce Manual and the Security Refernece Manual

 

best regards

Max

0 Kudos
Reply