RT117x: where is the FORCE_COLD_BOOT fuse reflected?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT117x: where is the FORCE_COLD_BOOT fuse reflected?

ソリューションへジャンプ
989件の閲覧回数
mastupristi
Senior Contributor I

On the Ref Man I read:

Screenshot_2023-04-11_18-15-01.png

the FORCE_COLD_BOOT should be reflected in SRC_SBMR...

I looked for SRC_SBMR and found two registers, but in neither of them do I seem to see the bit reflected by the FORCE_COLD_BOOT fuse.

Could you point me to which register and which bit I find it in?

best regards

Max

タグ(3)
0 件の賞賛
返信
1 解決策
966件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

This is true. Confirmed by support engineer.

 

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
973件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

For RT1170, I think this fuse bit is not touched by ROM. You can ignore it.

 

Regards,

Jing

0 件の賞賛
返信
969件の閲覧回数
mastupristi
Senior Contributor I

I think this fuse bit is not touched by ROM. You can ignore it.

Is this your feeling or do you have written confirmation in some document?
Because the only document I have available says the fuse is there and it's reflected somewhere on SRC.

 

best regards

0 件の賞賛
返信
967件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

This is true. Confirmed by support engineer.

 

Regards,

0 件の賞賛
返信
964件の閲覧回数
mastupristi
Senior Contributor I

Then I suggest removing the description of that fuse from both the Refernce Manual and the Security Refernece Manual

 

best regards

Max

0 件の賞賛
返信