RT117x - hyperFlash and hyperRam in same design?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT117x - hyperFlash and hyperRam in same design?

454件の閲覧回数
nickwallis
Senior Contributor I

hi,

Is it possible to have both hyperFlash and hyperRam in the same design (on different interfaces, not sharing the same interface).

Does this just come down to pin availability/pin muxing or are there other considerations?

The use case is we want to use the DMA controller to DMA data from some peripheral into buffers which would reside in external hyperRam, the external hyperFlash would be used for code execution.

many thanks!

 

タグ(1)
0 件の賞賛
返信
1 返信

444件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @nickwallis ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Does this just come down to pin availability/pin muxing or are there other considerations?
-- It's able to implement the above purpose, as the RT117x contains the 2 FlexSPI modules.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信