RT1172: CAAM init fail with encrypted OTFAD and HAB enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1172: CAAM init fail with encrypted OTFAD and HAB enabled

Jump to solution
691 Views
pieropischedda
Contributor I

Goodmorning.

I'm working with RT1172 cpu that manage an emmc memory. The software is working fine.

Now I'm testing the OTFAD encryption and the secure boot.

I'm using the MCUXpresso Secure Provisioning to flash the board. With the encrypted OTFAD authenticated and the HAB disabled all works fine. Now I enabled the HAB, the firmware starts but gets an error when CAAM_init is invoked. The function caam_out_job_ring_test_and_remove fails.

What's wrong? Are there any fuse that I'm missing to burn or are there any special configuration needed for CAAM when HAB is enabled?

Thanks

0 Kudos
Reply
1 Solution
515 Views
Kaidou
Contributor II

Hello.

It seems that the problem was that we were calling the CAAM_init function twice in the firmware with the encrypted OTFAD authenticated boot and the HAB enabled.
This generated an error when calling the CAAM_RNG_GenerateSecureKey function.
After removing the wrong CAAM_inti call, the CAAM initialized correctly.

Thanks for the answer anyway!

Is it possible to get support on this issue?
https://community.nxp.com/t5/i-MX-RT/IMXRT1172-flashloader-not-starting/m-p/1824091#M29233

Thanks!

View solution in original post

0 Kudos
Reply
3 Replies
516 Views
Kaidou
Contributor II

Hello.

It seems that the problem was that we were calling the CAAM_init function twice in the firmware with the encrypted OTFAD authenticated boot and the HAB enabled.
This generated an error when calling the CAAM_RNG_GenerateSecureKey function.
After removing the wrong CAAM_inti call, the CAAM initialized correctly.

Thanks for the answer anyway!

Is it possible to get support on this issue?
https://community.nxp.com/t5/i-MX-RT/IMXRT1172-flashloader-not-starting/m-p/1824091#M29233

Thanks!

0 Kudos
Reply
499 Views
diego_charles
NXP TechSupport
NXP TechSupport

Thanks for your response @Kaidou 

I will mark that as the answer. 

Sure, I am working on your other thread.

Best regards, 

Diego

0 Kudos
Reply
541 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @pieropischedda 

Thanks for reaching us. 
 
I still have not encountered this issue before. But want your help to dig further into this , could you provide me more details regarding the following?
 
-All the fuses that you already burned. 
- Do you see any failure with the CAAM_M7 or CAAM_M4 demos? 
 
Any other detail about your application is welcome. 
 
Thanks for your patience. 
Diego
 
0 Kudos
Reply