RT1062_uSDHC2-HS200驱动emmc5.0芯片异常

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1062_uSDHC2-HS200驱动emmc5.0芯片异常

3,623 Views
sunhonglisun
Contributor I

您好:

现在使用RT1062的uSDHC2驱动emmc5.0芯片(ISSI_IS21ES04G),使用官方SDK包提供的fsl_mmc的驱动底层;现在VCCQ =1.8V,配置High-speed时没有问题(实际速度49.5MHz;幅值也会有所减小);使用HS200模式驱动时(VCCQ =1.8V,实际配置为100MHz),引脚配置如下(附件:pin_mux.png):

pastedImage_3.png

emmc参数配置如下:

emmc->hostVoltageWindowVCC = kMMC_VoltageWindows270to360;
emmc->hostVoltageWindowVCCQ = kMMC_VoltageWindow170to195;
emmc->busTiming = kMMC_HighSpeed200Timing;
emmc->busWidth = kMMC_DataBusWidth8bit;

有时会初始化不成功,使用示波器抓了CLK引脚输出的波形,前期初始化波形的幅值为0.1-1.8V左右,示波器截图详见附件:emmc_1.bmp;切换100Mhz后幅值变小了在0.58-1.18V之间,示波器截图详见附件:emmc_100MHz.bmp;同时抓取了CMD和DAT0的波形幅值都在0.1-1.8V(最小值、最大值);如果将通讯时钟调到198MHz,几乎无法完成emmc初始化,经过对比认为是CLK引脚随着时钟频率升高幅值会继续下降,导致emmc无法完成初始化。

请问是什么原因导致 CLK引脚随着时钟频率升高幅值会继续下降?

Labels (1)
0 Kudos
Reply
2 Replies

3,463 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi sunhongli sun,

  楼主你好!

刚才我们论坛外也有些许问题的简单沟通。

大致总结是这样:

1. clk 99MHZ通信成功, 198Mhz失败

2. 176MHZ 也失败

3. CLK频率越高,低电平被太高,怀疑是这个电平被太高之后导致通信失败

4. CLK DATA两根线硬件使用同样的阻抗和走线,但是DATA电平信号正常。

5. 硬件走线50欧阻抗,引脚配置52阻抗

6. 跑198M, data 读写0XAA, data速率99M或者, 波形没有99Mhz clk信号那么差。

那么现在,楼主是否可以再提供如下几种波形:

1. CLK 99MHZ 波形

2. data 99Mhz, 也就是CLK 198Mhz, 这个示波器波形界面配置和CLK 99MHZ波形一样。好让我看到同样99MHz CLK 和DATA差异。

3. 198Mhz CLK的波形也给我放大版的,能看到具体幅度与频率那种。

另外,你有没有测试上100Mhz,最大能够初始化完成的频率?

100MHZ你那边是否能够成功?

我不知道你的示波器探头,是否会有高频抓取有干扰的情况?

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,463 Views
sunhonglisun
Contributor I

实际硬件走线已经做了50欧姆的阻抗匹配。

0 Kudos
Reply