RT1062 ASPI boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1062 ASPI boot

703件の閲覧回数
gregory_grzesia
Contributor I

Hi

We want to connect QSPI flash for booting,

Page 2 on 'Mitigation guide from i.MX RT1060 to i.MX RT1064 says that there is a number of of pins possible,

First section in table 1 states B and A modules, second states only A FLEXSPI module that is selectable by setting BOOT_CFG2[2:0] bits

Now on the first section of table 1,

Is it that I can connect my QSPI Flash either to module A or B or is it fixed to A or B, unchangeable?

If there is a choice between A and B where do I configure the device to start either from A or B?

Thanks,

Best

0 件の賞賛
返信
1 返信

668件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Gregory Grzesiak ,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is it that I can connect my QSPI Flash either to module A or B or is it fixed to A or B, unchangeable?
-- It should connect the FlexSPI_A channel.

Have a great day,

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信