RT1050 Rom Boot loader devices connections

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RT1050 Rom Boot loader devices connections

跳至解决方案
1,836 次查看
jamesli
Contributor IV

On the latest data sheet, when boot loader from UART1, Table 79 show 4 pins are used, 

pastedImage_1.png

But on reference manual table 8-1 as follows:

pastedImage_2.png

Only two pins are needed. Which one I should to use, if the UART1 port does not use CTS and RTS signals, is boot loader still to talk the device? Where I can find more information regarding the ROM bootloader?

When boot from FlexSPI, it lists a hyper flash as follows:

pastedImage_3.png 

Is the ROM boot loader works with QSPI flash on FLEXSPI_A or FLEXSPI_B port, if yes, how it behaviors? Which IC is selected first? FLEXSPI_A_SS0_B or  FLEXSPI_B_SS0_B? What is required connections?

Any  help is appreciated! Thank you in advance!

标记 (1)
0 项奖励
回复
1 解答
1,459 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Jian Li,

The ROM bootloader supports booting through UART with RX/TX only (no hardware flow control). Additionally, I do not know of any other documents with deep information on the ROM bootloader, but I will ask around and let you know if I find something useful. For instance you can take a look here:

https://www.nxp.com/docs/en/application-note/AN12107.pdf 


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,460 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Jian Li,

The ROM bootloader supports booting through UART with RX/TX only (no hardware flow control). Additionally, I do not know of any other documents with deep information on the ROM bootloader, but I will ask around and let you know if I find something useful. For instance you can take a look here:

https://www.nxp.com/docs/en/application-note/AN12107.pdf 


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,459 次查看
jamesli
Contributor IV

Hi, Carlos_Musich: Thank you for help and promise for more info.

0 项奖励
回复