RT1050 MCUXpresso GDB Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1050 MCUXpresso GDB Error

3,204 次查看
ryanshuttlewort
Contributor IV

Hello, I am trying to debug a simple hello world application on the MIMXRT1050-EVK using the MCUXpresso IDE.  Please see my previous post.

As of yesterday, Nov 16th, 2017 it appears that the RT1050 SDK now supports MCUXpresso IDE.  I am able to import and compile the simple hello world application, however, when I attempt to download and debug I get the GDB error shown below. 

Notes:

  • I am having no issue compiling, downloading and debugging from IAR on the same board.
  • MCUXpresso is running on Ubuntu 14.04

Initial error message:

Error in final launch sequence
Failed to execute MI command:
-target-select extended-remote | crt_emu_cm_redlink -msg-port=39099 --no-packed --cachelib libm7_cache.so -g -mi -2 -pMIMXRT1052xxxxx -vendor=NXP -reset= -ProbeHandle=1 -CoreIndex=0 -cache=disable -x /home/colby/Documents/MCUXpresso_10.0.2_411/workspace/evkmimxrt1050_demo_apps_hello_world_hello_world/Debug --flash-dir /home/colby/mcuxpresso/.mcuxpressoide_packages_support/MIMXRT1052xxxxx_support/Flash --telnet 3331
Error message from debugger back end:
Remote communication error.  Target disconnected.: Connection reset by peer.
Remote communication error.  Target disconnected.: Connection reset by peer.

eclipse.buildId=unknown
java.version=1.8.0_111
java.vendor=Oracle Corporation
BootLoader constants: OS=linux, ARCH=x86_64, WS=gtk, NL=en_CA
Command-line arguments:  -os linux -ws gtk -arch x86_64

org.eclipse.cdt.dsf.gdb
Error
Fri Nov 17 07:02:05 PST 2017
Failed to execute MI command:
-target-select extended-remote | crt_emu_cm_redlink -msg-port=39099 --no-packed --cachelib libm7_cache.so -g -mi -2 -pMIMXRT1052xxxxx -vendor=NXP -reset= -ProbeHandle=1 -CoreIndex=0 -cache=disable -x /home/colby/Documents/MCUXpresso_10.0.2_411/workspace/evkmimxrt1050_demo_apps_hello_world_hello_world/Debug --flash-dir /home/colby/mcuxpresso/.mcuxpressoide_packages_support/MIMXRT1052xxxxx_support/Flash --telnet 3331
Error message from debugger back end:
Remote communication error.  Target disconnected.: Connection reset by peer.

java.lang.Exception: Remote communication error.  Target disconnected.: Connection reset by peer.
     at org.eclipse.cdt.dsf.mi.service.command.AbstractMIControl$RxThread.processMIOutput(AbstractMIControl.java:940)
     at org.eclipse.cdt.dsf.mi.service.command.AbstractMIControl$RxThread.run(AbstractMIControl.java:769)
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

GDB console dump (error at end):

922,111 2-list-thread-groups
922,111 2^done,groups=[{id="i1",type="process"}]
922,113 (gdb) 
923,410 3-gdb-version
923,412 ~"GNU gdb (GNU Tools for ARM Embedded Processors) 7.12.0.20161204-git\n"
923,413 ~"Copyright (C) 2016 Free Software Foundation, Inc.\n"
923,413 ~"License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>\nThis is fre\
e software: you are free to change and redistribute it.\nThere is NO WARRANTY, to the extent permitt\
ed by law.  Type \"show copying\"\nand \"show warranty\" for details.\n"
923,413 ~"This GDB was configured as \"--host=x86_64-linux-gnu --target=arm-none-eabi\".\nType \"sho\
w configuration\" for configuration details."
923,413 ~"\nFor bug reporting instructions, please see:\n"
923,413 ~"<http://www.gnu.org/software/gdb/bugs/>.\n"
923,413 ~"Find the GDB manual and other documentation resources online at:\n<http://www.gnu.org/soft\
ware/gdb/documentation/>.\n"
923,413 ~"For help, type \"help\".\n"
923,413 ~"Type \"apropos word\" to search for commands related to \"word\".\n"
923,413 3^done
923,413 (gdb) 
923,414 4-environment-cd /home/colby/Documents/MCUXpresso_10.0.2_411/workspace/evkmimxrt1050_demo_ap\
ps_hello_world_hello_world
923,415 4^done
923,415 (gdb) 
923,416 5-gdb-set breakpoint pending on
923,417 5^done
923,417 (gdb) 
923,418 6-enable-pretty-printing
923,419 6^done
923,419 (gdb) 
923,419 7-gdb-set python print-stack none
923,419 7^done
923,419 (gdb) 
923,420 8-gdb-set print object on
923,420 8^done
923,420 (gdb) 
923,420 9-gdb-set print sevenbit-strings on
923,421 9^done
923,421 (gdb) 
923,421 10-gdb-set charset ISO-8859-1
923,422 10^done
923,422 (gdb) 
923,422 11-gdb-set auto-solib-add on
923,422 11^done
923,422 (gdb) 
923,425 12-file-exec-and-symbols --thread-group i1 /home/colby/Documents/MCUXpresso_10.0.2_411/works\
pace/evkmimxrt1050_demo_apps_hello_world_hello_world/Debug/evkmimxrt1050_demo_apps_hello_world_hello\
_world.axf
923,429 12^done
923,429 (gdb) 
923,432 13-interpreter-exec console "set non-stop on"
923,432 =cmd-param-changed,param="non-stop",value="on"
923,432 13^done
923,432 (gdb) 
923,434 14-interpreter-exec console "set pagination off"
923,434 =cmd-param-changed,param="pagination",value="off"
923,435 14^done
923,435 (gdb) 
923,441 15-interpreter-exec console "set mi-async"
923,442 =cmd-param-changed,param="mi-async",value="on"
923,443 15^done
923,443 (gdb) 
923,446 16-interpreter-exec console "set remotetimeout 60000"
923,446 =cmd-param-changed,param="remotetimeout",value="60000"
923,447 16^done
923,447 (gdb) 
923,817 17-target-select extended-remote | crt_emu_cm_redlink -msg-port=39099 --no-packed --cachelib\
 libm7_cache.so -g -mi -2 -pMIMXRT1052xxxxx -vendor=NXP -reset= -ProbeHandle=1 -CoreIndex=0 -cache=d\
isable -x /home/colby/Documents/MCUXpresso_10.0.2_411/workspace/evkmimxrt1050_demo_apps_hello_world_\
hello_world/Debug --flash-dir /home/colby/mcuxpresso/.mcuxpressoide_packages_support/MIMXRT1052xxxxx\
_support/Flash --telnet 3331
923,827 &"Ea: Unrecognized option: --no-packed\n"
923,827 17^error,msg="Remote communication error.  Target disconnected.: Connection reset by peer."
923,828 (gdb) 
923,834 18-target-disconnect
923,834 19-gdb-exit
923,835 18^error,msg="You can't do that when your target is `exec'"
923,836 (gdb) 
923,836 19^exit‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Here is the output from the RedLink server console:

[Started server]
[Connected on port 3025]
redlink>ProbeList
Index = 1
Manufacturer = ARM
Description = DAPLink CMSIS-DAP
Serial Number = 0225000041114e450025300ac207002a92d1000097969900
VID:PID = 0D28:0204
Path = /dev/hidraw1
redlink>ProbeStatus
Index = 1
Manufacturer = ARM
Description = DAPLink CMSIS-DAP
Serial Number = 0225000041114e450025300ac207002a92d1000097969900
VID:PID = 0D28:0204
Path = /dev/hidraw1
IsOpen = FALSE
WireInitialized = FALSE
WireProtocol = JTAG
CoresConfigured = FALSE
PacketSize = 64
Reference Count = 0
HasSWV = FALSE
HasETM = FALSE
HasJTAG = TRUE
HasSWD = TRUE
Probe Type = CMSIS-DAP
Probe Reference Count = 0
redlink>ProbeIsOpen 1
FALSE
redlink>ProbeOpenByIndex 1 
Probe Handle 1 Open
redlink>WireIspReset 1
redlink>WireIsConnected 1
FALSE
redlink>WireSwdConnect 1
DpID = 0BD11477
redlink>CoresConfigured 1
FALSE
redlink>CoreConfig 1
Number of CORES/TAPs = 1, Fully recognized: True
redlink>ProbeStatus
Index = 1
Manufacturer = ARM
Description = DAPLink CMSIS-DAP
Serial Number = 0225000041114e450025300ac207002a92d1000097969900
VID:PID = 0D28:0204
Path = /dev/hidraw1
IsOpen = TRUE
WireInitialized = TRUE
WireProtocol = SWD
CoresConfigured = TRUE
PacketSize = 64
Reference Count = 0
HasSWV = FALSE
HasETM = FALSE
HasJTAG = TRUE
HasSWD = TRUE
Probe Type = CMSIS-DAP
Probe Reference Count = 0
redlink>quit
[Closed]‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Any insight into how to correct the issue would be appreciated, thanks.

标签 (1)
标记 (4)
0 项奖励
回复
2 回复数

2,374 次查看
ryanshuttlewort
Contributor IV

An update for anyone having this issue. It seems that this issue is specific to the RT1050 and MCUXpresso v10.0.2, upgrading to v10.1.0 has corrected this issue.  Unfortunately the v10.0.2 "Check for updates" feature doesn't seem to be functional as it reports that no updates are available.  I had to download the latest MCUXpresso version and re-install.  

2,374 次查看
pradnyamane
Contributor I

Thanks Ryan,

            Changing the IDE helped.

0 项奖励
回复