Dear NXP group
I reference SDK "SDK_2_13_0_MIMXRT1052xxxxB to use RT1052 mcu,the LVGL project seems have some errors,when i display a image with PXP macro enable,the screen will blink,when i disable PXP macro,LVGL display the image correctly,the image need tarnsform into c array,is there anything wrong with the PXP configration?
Hello @InvisibleWind,
Could you please try using the SDK_2_14_0_MIMXRT1052xxxxB? Are you using our EVK or a custom board?
Also, are you using an example or a custom code? If you are using a custom code, could you please try the LVGL and PXP examples? Is the same issue happening there?
Finally, could you please tell us which screen are you using?
Best regards, Raul.