RT1050-EVKB run from QSPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1050-EVKB run from QSPI

ソリューションへジャンプ
444件の閲覧回数
dinocroc123
Contributor II

Hey people,

i have an RT1050-EVKB board and want to run code from the QSPI memory.

I can configure read/write/erase it via mcuexpresso but when trying to debug there is a hardfault.

Also the flash downloadspeed is reported as 1000KB/s which cannot be.

I'm using the MIMXRT1050-EVK_IS25WP064A.cfx driver.

Is there a step-by-step guide on how to configure a project to run from the QSPI?

I'm also confused about the function of the xip folder that is generated with my project. There is a "hyperflash_config" structure, but i cannot find "qspi_config" one.

Thank you!

 

0 件の賞賛
返信
1 解決策
441件の閲覧回数
dinocroc123
Contributor II
0 件の賞賛
返信
1 返信
442件の閲覧回数
dinocroc123
Contributor II
0 件の賞賛
返信