RT1050-EVKB run from QSPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1050-EVKB run from QSPI

Jump to solution
1,063 Views
dinocroc123
Contributor II

Hey people,

i have an RT1050-EVKB board and want to run code from the QSPI memory.

I can configure read/write/erase it via mcuexpresso but when trying to debug there is a hardfault.

Also the flash downloadspeed is reported as 1000KB/s which cannot be.

I'm using the MIMXRT1050-EVK_IS25WP064A.cfx driver.

Is there a step-by-step guide on how to configure a project to run from the QSPI?

I'm also confused about the function of the xip folder that is generated with my project. There is a "hyperflash_config" structure, but i cannot find "qspi_config" one.

Thank you!

 

0 Kudos
Reply
1 Solution
1,060 Views
dinocroc123
Contributor II
0 Kudos
Reply
1 Reply
1,061 Views
dinocroc123
Contributor II
0 Kudos
Reply