I am using the IMX RT1021 microcontroller.
I'm trying to configure the LPUART interface to read IR codes.
I saw that there are no examples available and I noticed that the SDK doesn't seem to be supported.
I found a post on the Forum similar to my need:
https://community.nxp.com/t5/i-MX-RT/Support-IrDA-in-SDK-API-for-RT1011-RT1015-MCUs/m-p/1045409
However it appears that the post did not conclude with a solution.
I'm in need of assistance.
Best regards.
Hello, my name is Pavel, and I will be supporting your case, I suggest downloading the example mentioned on the thread.
Emulating IRDA with the FlexIO on RT1010 (nxp.com)
You can find the project on this link i.MX RT1010 | Crossover MCU with ARM Cortex-M7 up to 500 MHz | NXP Semiconductors in the section of the documentation.
Best regards,
Pavel
Many thanks for the reply.
I've already seen this example using FlexIO.
However, I want to do it through the LPUART interface, as I mentioned previously.
Could you tell me if it is possible and how should I proceed?
Hello, sorry I´m not familiar with IRDA but I reviewed the note app is using the FlexIO_UART, and maybe will is not difficult to migrate to the LPUART, I suggest reviewing how is the example works in bare metal I mean need to debug the example and review what is the example doing on the register on the TX and RX and replayed.
Best regards,
Pavel