RT1020 XIP Firmware update

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1020 XIP Firmware update

1,264 次查看
hacksome
Contributor I

Hi All

Our custom board is being laid out that will use the RT1020 running from a IS25WP064 Serial Flash Memory. We don't have SDRAM attached do it will be running ins XiP mode using the internal ram only. Can some one tell me if this is a good way to do it? Can you for see any problems. Our application doesn't need much RAM .  

Also we have another processor on board that talks to to wifi and will be able to download new firmware images for the RT1020. Our plan is to load the image using the serial boot loader into the Flash Memory. Do you think this will work?

Thanks

标签 (1)
0 项奖励
回复
1 回复

832 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Taimur

yes one can use XiP mode using the internal ram only, may be useful to check

White Paper: Memory Expansion with Adesto EcoXIP and i.MX RT,
using MCUXpresso on Figure 11: Selecting Adesto Serial Flash
https://www.nxp.com/docs/en/white-paper/NXPADESTOWP.pdf 

For loading the image into the Flash Memory one can look on

AN12238 i.MX RT Flashloader Use Case

https://www.nxp.com/docs/en/nxp/application-notes/AN12238.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复